cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK-V3 support in STM32CubeIDE?

Jan1
Associate II

Hello,

I just bought a STLINK-V3 because of its faster USB interface to speed up debugging with STM32CubeIDE. Unfortunately I cannot get it working. With some settings the target is not found with others there are errors during flash programming. Does STM32CubeIDE support this debugger at all? If yes, is there a description how to set it up?

The STLINK-V3 works fine with STM32CubeProgrammer.

Regards

Jan

1 REPLY 1
Gabriele1
Associate II

Hi Jan,

I think it is supported. I'm using a NUCLEO-144 board with ST-LINK v3 embedded on it and it's working fine. Check for updates of ST-LINK and STM32CubeIDE.