cancel
Showing results for 
Search instead for 
Did you mean: 

Stlink-v3-minie upgrade

oeliks
Senior

Hi! When I connect stlink v3 minie , lounch cubeide -> stlink upgrade , it only shows "V3",  nothing more. I can't open it for upgrade.

Other embedded in nucleo boards stlink v3 works and can be upgraded (nucleo G431 and H723).

There is an error about permissions. But I don't think that's the case.

Its brand new device, never used, never connected to target, original.

There is possibility that cubeide didn't updated - so I will try to download latest and update. But chances are small for this.

What to try first?

Thanks.

 

Edit: it was indeed a failed update issue. Solved!

2 REPLIES 2
Pavel A.
Evangelist III

Do the update on a good Windows 10 or 11 PC, with good cables. Using the latest Cubeide version is a good idea.

 

 

NO WAY ! I will stick with linux. It updates with no problems now.