2021-08-20 2:15 PM
I can't get the STLink drivers installed on Windows 10 / 11 aarch64 Parallels VM running on Mac M1.
Is there any support for ARM64 Windows STLink drivers?
Solved! Go to Solution.
2024-01-31 6:13 PM
Thank you, this worked perfectly on my Windows 11 inside parallels on an M1 Macbook pro.
2024-07-07 11:06 AM - edited 2024-07-09 5:30 AM
Thank you, this worked flawlessly following strictly the steps.
2024-12-21 9:30 PM
Three years after CPop.1's post, these instructions and the zip file in CPop.1's post worked great for me. Here is my configuration.
Apple M1 Max, Sequoia 15.2 (24C101)
Parallels Desktop Version 20.1.3 (55743)
Microsoft Windows 11 Home, 22H2, 64-bit operating system, ARM-based processor
STM32 Cube Programmer v2.18.0
2025-01-01 8:27 PM
For some reason I am still struggling with this. I bought Surface Pro recently
Config:
Windows 11 Home (Version 24H2)
System: 64-bit OS, ARM processor
Processor: Snapdragon X10-Core
I installed STM IDE and trying to work on STM32L476RG MCU, but USB driver is not working. I disable Digital Driver Signing and secure boot. After spending hours, I was about to install drivers but it installs as AMD64 driver.. when I plug board it doesn't recognize installed drivers. I tried updating driver manually but it doesn't show up in the list as well. Can you please help as I need to work on a few projects using this board?
2025-01-02 12:58 PM
Thanks to you, I managed to install driver on Windows 11 ARM64 (Surface Pro) but for some reason STM IDE still doesn't recognize it.. Also I noted that device shows up as "Other Devices" not USB device. Do I need to do anything or change any config to have it recognized as valid device on STM IDE?
2025-01-03 6:30 AM
Hi @Mparikh06 ,
Can you connect with STM32CubeProgrammer?
Check some hints to recognize a genuine ST-Link V2.