2024-12-14 04:35 PM
Is there ST-Link V2 driver for Windows 11? I am using Microsoft Surface Pro + Copilot and trying to load code on STM32L476.
2024-12-14 05:42 PM - edited 2024-12-14 05:43 PM
What do you see in the device manager when the ST-Link is connected? (View->Devices by container)
2024-12-18 06:15 PM
The USB drivers for the STLINK-Vx (STSW-LINK009)
https://www.st.com/en/development-tools/stsw-link009.html
it mentions "USB driver signed for Windows7, Windows8, Windows10". it works on my PC with Win11 (Windows 11 Enterprise, Version 23H2) also.
2025-01-01 08:29 PM
For some reason I am still struggling with this. I bought Surface Pro recently
Config:
Windows 11 Home (Version 24H2)
System: 64-bit OS, ARM processor
Processor: Snapdragon X10-Core
I installed STM IDE and trying to work on STM32L476RG MCU, but USB driver is not working. I disable Digital Driver Signing and secure boot. After spending hours, I was about to install drivers but it installs as AMD64 driver.. when I plug board it doesn't recognize installed drivers. I tried updating driver manually but it doesn't show up in the list as well. Can you please help as I need to work on a few projects using this board?
2025-01-01 11:49 PM
It seems that no official ARM64 Windows STLink driver is available. Perhaps you may try some workaround found from internet.
@AM Could you please help to clarify ?
2025-01-02 01:14 AM
I confirm the issue is linked to Windows ARM64 OS not yet supported by official ST-Link USB driver.
You may have a look at this topic which is the same issue:
Best regards
2025-01-02 01:00 PM