2025-02-19 12:46 AM
Hello,
we have purchased multiple Nucleo H723ZG and H7A3ZI-Q. Since the beginning, connection problems with ST-Link are plaguing the project. It is impossible to reliably debug, because connection with the host can't be established via USB. We have checked all possible sources (like different computers, cables, docks, ports, software, et.c.), but the issue sporadically appears, even with brand new boards out of the box, which costs money. Other users face similar issues and I wonder what steps ST wants to take.
Best regards
2025-02-19 03:48 AM - edited 2025-02-19 03:53 AM
This smells like grounding issues. :D
>>Other users face similar issues and I wonder what steps ST wants to take.
I personally never had those issues, stlinks old and new are realiable.
Seeing your other posts it looks like youre getting started with ST, my money is on burnt nucleo board due to high voltage apølied to analog pins or defective project grounding.
Show us some pictures
Try this, use stlink with a laptop Pc unplugged from its wall charger, do your problems magically solve?
Are you conecting something else to your Nucleo H723ZG, maybe a oscilloscope probe?
2025-02-19 05:27 AM
Something with your setup isn't right. You shouldn't be having problems with debugging. More clarity into the setup and the exact problems you're having (exact error messages, etc) would be helpful. Unlikely that this is a board problem.
2025-02-19 06:34 AM
2025-02-19 02:55 PM
Connect the board thru a good USB 2.0 hub. Powered hub is even better.
2025-02-19 05:38 PM
As everyone seem to state, there must be something wrong with your setup. I've never had an issue with the Nucleo-H723ZG.