User Activity

Hello,we have purchased multiple Nucleo H723ZG and H7A3ZI-Q. Since the beginning, connection problems with ST-Link are plaguing the project. It is impossible to reliably debug, because connection with the host can't be established via USB. We have ch...
Dear all,in a project which was assigned to me with the NUCLEO-H723ZG, I have multiple digital outputs, like PG12, PE9, PE11, PE14, PE13, PG14 et.c. mostly originating from the CN10 ZIO connector, where the pin names are intuitive, e.g. D7, D6, D5, e...
Dear community, my Nucleo H723ZG captures analog signals via channels (see attachment) :ADC12_INP15,ADC12_INP10 andADC12_INP10 The second one reads a 4-20mA pressure signal from a sensor with the help of an external shunt resistor. After a system res...
Kudos given to