cancel
Showing results for 
Search instead for 
Did you mean: 

Specification of STDC16/MIPI10 Connector on Stlinkv3xx

Uwe Bonnes
Principal III

Hello,

e.g. the BOM for the NUCLEO-G474RE does not list CN4, what the manuals call "STDC14/MIPI". It is obvious that is is a 14-pin, 1.27 mm pitch connector with polarization. However having exact specification would help to buy fitting mates.

Some similar question "STDC14 connector name in STLINK-V3SET" went by unanswered in Dec 18.

3 REPLIES 3
Uwe Bonnes
Principal III

Shuffling up the question again.

kurta999
Senior

Any news on this? I have a G4 too and would like to buy a connector to that. I would like to use it's ST-Link V3.

Uwe Bonnes
Principal III

The schematics is now available as  mb1367-g474re-c04_schematic.pdf and CN4 is visible on page 7/8