2019-07-19 05:59 AM
Hello,
e.g. the BOM for the NUCLEO-G474RE does not list CN4, what the manuals call "STDC14/MIPI". It is obvious that is is a 14-pin, 1.27 mm pitch connector with polarization. However having exact specification would help to buy fitting mates.
Some similar question "STDC14 connector name in STLINK-V3SET" went by unanswered in Dec 18.
2019-07-29 01:43 AM
Shuffling up the question again.
2020-05-27 03:56 AM
Any news on this? I have a G4 too and would like to buy a connector to that. I would like to use it's ST-Link V3.
2020-05-27 04:20 AM
The schematics is now available as mb1367-g474re-c04_schematic.pdf and CN4 is visible on page 7/8