2021-05-28 03:44 AM
I am working with IAR EWARM 9.10.1 and STM32CubeMX 6.2.1 on a NUCLEO-H743ZI2.
To reproduce:
STM32CubeMX generation falsely changes the EWARM/<projectname>.ewd file, when working with modified EWARM project files.
<option>
<name>CCSTLinkProbeList</name>
<version>1</version>
<state>3</state> //this needs to stay at 3 for the NUCLEO-H743ZI2, but gets changed to 2
</option>
3 -> ST-Link V3
2 -> ST-Link V2
I am happy to help, as this is really annoying for my daily work.
Solved! Go to Solution.
2021-06-02 04:07 AM
Hi again @FZida.1 ,
I reproduced the issue and I confirm it, each time the code is re-generated, the <state>X</state> needs to conserve the change made by user.
I would like to take this opportunity to explain you the writing done in this configuration, in fact, the <state>0</state> means STLINK 1, <state>1</state> means STLINK2 and <state>2</state> means STLINK3.
Thanks @FZida.1 for reporting the problem, issue will be fixed.
Khouloud
2021-06-02 02:58 AM
Hello @FZida.1
Thank you for your post,
I'll check it then I'll get back to you :)
Khouloud
2021-06-02 04:07 AM
Hi again @FZida.1 ,
I reproduced the issue and I confirm it, each time the code is re-generated, the <state>X</state> needs to conserve the change made by user.
I would like to take this opportunity to explain you the writing done in this configuration, in fact, the <state>0</state> means STLINK 1, <state>1</state> means STLINK2 and <state>2</state> means STLINK3.
Thanks @FZida.1 for reporting the problem, issue will be fixed.
Khouloud