cancel
Showing results for 
Search instead for 
Did you mean: 

Programmer for Steval-IDP004V2 with the help of st link v3 mini

GVall.2
Associate II

Hallo Support Team,

i have a "STEVAL-BFA001V2B" kit containing

  • STLINK-V3MINI debugger/programmer for STM32 and STDC14 flat cable. 
  • One adapter for ST-LINK programming and debugging tool - STEVAL-UKI001V2.

and i had also the  STEVAL-IDP004V2 master board which has a ST Link V2 programmer, is it possible to use ST Link v3 mini for programming/Debugging " STEVAL-IDP004V2" , do i need another adapter for st link V2 20 pin?.

Thanking you.

Kind Regards,

Govil

1 REPLY 1
TDK
Guru

You'll need an adapter since the STLINK-V3MINI only has the 0.050" pitch cable connector, but the STLINK-V3MINI can be used as a programmer.

If you feel a post has answered your question, please click "Accept as Solution".