cancel
Showing results for 
Search instead for 
Did you mean: 

Error: No STM32 target found! on custom board

VCasa.4
Associate II

Hi,

I have designed a custom board based on a F417, I am trying to program it with an ST-Link V2 through SWD(SWCLK, SWDIO, GND and RST) and I only get: Error: No STM32 target found!

I have tried the CubeProgrammer, the STLink Utility, the CubeIDE, with modes Normal, Under Reset, Power Dowm... and nothing works.

The PCB traces are connected directly from the SWD header to the pins, but I have also tried with some PullUp-Down resistor on the lines, as a few designs have, and nothing...

I attach a screencapture of the PCB design file, 4 layers, used top and bottom for signals, 2nd for GND and 3rd for 3.3V, 100nF for each VDD pin...

I have tested all the sldering, and it is correct too.

I don't know what can I do from now.

Thank you so much

Best regards

0693W00000ANSk8QAH.png

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5

Likely an implementation detail rather than the tools. Indicating the part is currently in a non-functioning state.

Review Schematic

Check Orientation

Check supplies, especially VDDA / VSSA

Check VCAP pins and capacitors 2.2uF, 1.25V ?

Check voltage level observed on NRST

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
VCasa.4
Associate II

Hi,

I think that orientation is correct, point mark of the chip at the pin 1 corner.

VDDA is filtered by a FB and a 100nF from 3.3V, VSSA to GND.

VCAP 2.2uF for each VCAP pin, and 3.3V measuded when powered.

NRST behaves well, pulled high, filtered near the chip with 100nF.

Thank you

An authenticate/external ST-LINK/V2 expects pin 1 or 2 of the 20-pin header to be provided with the Target's supply voltage, VTarget = VCC 3.3V

The tools should report the voltage observed.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Yes, the softwares report 3.21V, I think that the problem is on V_CAPs, I have wired them to VCC bypassed with 2.2uF, but they don't go to 3.3V.

I will try to modify it, and will keep you updated.

Thank you so much!

TDK
Super User

> I think that the problem is on V_CAPs, I have wired them to VCC bypassed with 2.2uF, but they don't go to 3.3V.

V_CAP should not be tied to VCC. They are nominally ~1.2V.

If you feel a post has answered your question, please click "Accept as Solution".