2024-01-31 5:17 AM
Hello,
I am working the nucleo board ,similarly my led is blinking at 1 Hz , I want to use power bank through the USB connector for my power supply, My power bank output is 5v ,2A . In the user manual it was mentioned as if you not want to use usb enumeration put the jumper j1 as ON , and also mentioned to take care that input should not exceed 100 mA.
In my case jumper j1 is off and jumper 5 is on the usb power supply. what happen when I give 2 A power supply to the board by putting j1 as ON . Is there any other way to do it.
2024-01-31 5:22 AM
@srinath wrote:My power bank output is 5v ,2A .
That just means that your power bank is capable of supplying up to 2A.
A power supply (including a power bank) can't "force" more amps into a load than the load requires!
2024-01-31 5:26 AM
Current drawn will depend on the presented load, surely?
2024-01-31 6:41 AM - edited 2024-01-31 6:42 AM
@srinath wrote:I am working the (sic) nucleo board
There are many different Nucleo boards - which one are you using?
@srinath wrote:also mentioned to take care that input should not exceed 100 mA.
Are you referring to this:
Again, that is talking about how much the Nucleo board (and any attached shields) draws - which has nothing to do with the current rating of the power supply (eg, the 2A on your powerbank).
2024-01-31 8:24 PM
yes I am referring to this , Is it the max current allowed ? and my load will be around 500 mA . If I put the jumper J1 on and connect the power supply to power band using USB , does it able to draw the current ? and any tips and suggestion will most welcoming and thank you the quick reply.
2024-02-01 1:54 AM
Did you read the bit about the USB Enumeration?
That explains the 100mA limit.
Almost certainly, your power bank won't do USB enumeration - it just acts like a dumb power supply.