cancel
Showing results for 
Search instead for 
Did you mean: 

The stm32 is not supplied with current.

Julia_kwon
Associate

Hi, I designed stm32f413RGT6. But when I supplied 5V as a power supply, I only get 0.00~0.01A.
When I measure with a multimeter, the chip has a voltage of 3.3V.
I think it's a problem caused by not connecting VCAP1, so I connected 4.7uF to VCAP1 with GND, but the problem is the same.
Can you help me?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Check you see 1.25V at VCAP pin

Check part orientation 

Check level on NRST

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

On the nrst pin, when you open the switch, when you close the 3.3V switch, 0V comes out normally.
Also, there is no problem with the direction of the parts.
1.13V is measured in VCAP1, is there a problem with this?