cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo MB1364 as standalone ST-Link V3

DrDro
Associate III

Hi there,

I have developed my project long time with MB1364E, exactly with H723ZG.

Now I have got my own PCB with H743. I would like to use ST-Link V3 (SWD) from Nucleo board just the same as it works for cuttable ST-Link from L4 Nucleos, e.g.:
https://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-use-the-standalone-st-link-capability-of-my-nucleo-after/td-p/306461

I have removed JP4 "Idd measurement", JP2 "Power source selection" and JP5 "Power selection".

But it seems that Nucleo ST-Link is hardcoded to support only this board.
Log from CubeProgrammer:

 

  07:59:18:504 : UR connection mode is defined with the HWrst reset mode
  07:59:20:007 : ST-LINK SN  : 003600453331510B33323639
  07:59:20:007 : ST-LINK FW  : V3J12M3
  07:59:20:008 : Board       : NUCLEO-H723ZG
  07:59:20:008 : Voltage     : 3.29V
  07:59:20:008 : Error: ST-LINK error (DEV_TARGET_HELD_UNDER_RESET)
  07:59:20:024 : Disconnected

 

 However, when my PCB is not supplied I get another error from CubeProgrammer, the voltage is correctly 0.00V detected:

 

  08:03:06:200 : UR connection mode is defined with the HWrst reset mode
  08:03:06:234 : ST-LINK SN  : 003600453331510B33323639
  08:03:06:234 : ST-LINK FW  : V3J12M3
  08:03:06:235 : Board       : NUCLEO-H723ZG
  08:03:06:235 : Voltage     : 0.00V
  08:03:06:235 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
  08:03:06:249 : Disconnected

 

Yes, I can still work with external ST-Link V3 and my board. But I also want to reuse part of not anymore used NUCLEO board.

Let's say, just to reduce garbage and save the world.
Is there a way to free the ST-Link V3 from NUCLEO board?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Super User

looking at the circuit (MB1364) , the H723 is fix connected to the st-link F723.

so no easy way to use it.

you could try cutting the connections swdio, swclk, swo (sb32) close to the H723 and use the CN5 pinheader to connect a cable.

but maybe it expect just a H723 as target...and refuses to work with other.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
AScha.3
Super User

looking at the circuit (MB1364) , the H723 is fix connected to the st-link F723.

so no easy way to use it.

you could try cutting the connections swdio, swclk, swo (sb32) close to the H723 and use the CN5 pinheader to connect a cable.

but maybe it expect just a H723 as target...and refuses to work with other.

If you feel a post has answered your question, please click "Accept as Solution".
FBL
ST Employee

Hello @DrDro 

Check the user manual STM32H7 Nucleo-144 boards (MB1364) - User manual

It should be helpful as well.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

>> but maybe it expect just a H723 as target...and refuses to work with other.

I'm not aware about such a limitation, so far...

Anyways, for that board, the use case is that you can only bring an external probe to debug the H723, but can't debug an external MCU with the on-board ST-Link V3.

Maybe it is possible, but as you said, there is some work to do with cutter/soldering iron.