cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo H723ZG docking options

Lysandros
Associate II

Hello,

I want to use the Nucleo H723ZG for a project with analog & digital lines and can't find the article number of the headers CN7, CN8, CN9, CN10. Is there a specific cable/contact type I can use to plug in the black header body? Or are the headers pins at the bottom of the board meant to dock on some connector? Are there recommended docker boards like from Seeed Studio?

Many thanks 

2 REPLIES 2
SofLit
ST Employee

Hello,

Not pretty clear  ..

The CNx pinout description are provided in UM2407 Table 18 to Table 21.

You can develop your own board that fit these connectors and plug the Nucleo to it.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

You mean what ST call the "Zio" connectors:

AndrewNeil_0-1718011951219.png

As it says there, these will mate with standard ARDUINO® Uno V3 shields - so they are just 0.1" pitch headers, on the Arduino layout.