cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-f446RE: external power supply while using UART and STLINK virtual comport

harry123
Senior II

HI Everyone

  • I am using Nucleof446RE board for uart communication through usb cable which is also my power supply
  • Is it possible to use external 5V supply for MCU and use USB cable only for uart communication or any uart to usb converters are needed to communicate to PC.

Thank you

1 ACCEPTED SOLUTION

Accepted Solutions
QSHAO.1
ST Employee

with setting of jumper JP5, you are allowed to select power supply either from USB connector CN1 or from VIN (pin8) of Arduino connector CN6.

so you just need to set JP5 to 2-3, and connect external DC power to VIN pin (7-12V) to power your board.

View solution in original post

2 REPLIES 2

AndrewNeil_0-1728034381590.png

 

Also check the schematics...

QSHAO.1
ST Employee

with setting of jumper JP5, you are allowed to select power supply either from USB connector CN1 or from VIN (pin8) of Arduino connector CN6.

so you just need to set JP5 to 2-3, and connect external DC power to VIN pin (7-12V) to power your board.