cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-F103RB startup with the ST-Link disconnected adds delay

Kmax18
Senior

The below oscilloscope capture appears to show that disconnecting the ST-Link from the Windows laptop adds 80 ms to the NUCLEO startup, until the first UART packet is sent. If that is correct, what can cause this delay?

Thank you in advance for your feedback!

Kmax18_0-1692161680305.png

2 REPLIES 2
TDK
Guru

How are you assessing t=0 here? I see nothing to provide a time reference. Perhaps also capture NRST.

In any case, ST-Link will only affect code execution if it's being utilized.

If you feel a post has answered your question, please click "Accept as Solution".
jiangfan
ST Employee

The context is not clear. what are the board power settings for your comparison?