cancel
Showing results for 
Search instead for 
Did you mean: 

Need help with determining pinout of STMod+ ext. board on STM32H750B-DK board

bully
Senior

Hello,

I'd kindly ask for some help on determining exactly which MCU pin is connected to STMod+ extension board.

Which pins exactly are connected to STMod+ pins 2 and 3 ?

It seems like two choices for both pins, but I'm not sure how to check/modify which comes to STMod+ connector?

I guess from schematic that PI2 amd PB15 are connected to pins 2 NS 3, but that would mean that I don't have 

USART device on STMod+ connector ?

Thanks in advance,

regards.

 

2024-05-02 12_54_29-en.MB1381-H750XB-B01_Schematic - PDF-XChange Viewer.png

10 REPLIES 10

Agree, not usable for Clickboards, but usable for breadboard connections and prototyping.

 

Regards.