2024-06-26 07:28 PM
Hi guys,
Just wonder if there is anyone tried LwIP on the newer version of stm32cubeIDE (1.12 and above). I am trying to integrate stm32F4 series with LAN8720.
There is a "Platform settings" which requires us to select the driver_PHY. I am using LAN8720 but I can only see "Undefined, LAN8742 and DP83848" as options.
I went thru UM1709, UM1713, UM1718 and AN3966 but still could not find the solution. At least UM1718 section 19.10 still mentioned there should be a "user PHY" but this option is not available in my current version of IDE.
Maybe I should just try to modify LAN8742's BSP driver's code? or is there anyway I could manually include the component drivers to be used in my project? If yes, may I know how? (Newbie to ethernet protocol)