cancel
Showing results for 
Search instead for 
Did you mean: 

Keil project compilation error in NUCLEO-H755ZI-Q

KevinNapier
Associate II

i'm using the AC6.16 compiler and keil 5.34.

i'd like to use DMA in UART,and the file dma.c occured in both CM4 and CM7 folder(UART is attached to cortex-m4).but when i want to compile CM4 and CM7 project,both have said that "multiply defined".

KevinNapier_0-1717771915609.png

how can i do to resolve?thx.

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

In your project you added two dma.c file instances and that's normal. You need to add just one dma.c instance to your project as a common file. You can separate it from CMx/Core tree.

For example:

system_stm32h7xx.c is a common file for both CM4 and CM7:

SofLit_0-1718010823654.png*

See STM32H7 Cube package in github: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/NUCLEO-H745ZI-Q/Examples/GPIO/GPIO_EXTI/Common/Src

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

In your project you added two dma.c file instances and that's normal. You need to add just one dma.c instance to your project as a common file. You can separate it from CMx/Core tree.

For example:

system_stm32h7xx.c is a common file for both CM4 and CM7:

SofLit_0-1718010823654.png*

See STM32H7 Cube package in github: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/NUCLEO-H745ZI-Q/Examples/GPIO/GPIO_EXTI/Common/Src

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.