2022-06-26 04:36 AM
Hello,
Is there a way to use a ST-LINK/V2 from a Windows 11 machine? The device is not recognized when I connect it to the computer. The specifications indicate that the official support does not exceed Windows 10. The latest drivers have successfully been installed on my computer but the ST-LINK/V2 is not recognized. I tried to manually install the .inf file too, but to no avail.
EDIT: I got it to work by programming my board via a STM32F1 Discovery board (used as a programmer) circumventing the ST-LINK/V2 entirely.
2022-06-26 12:31 PM
Yes, it is fully supported. Just install the current driver supplied with STM32CubeIDE or STM32 CubeProgrammer, not the old stuff from .zip files. Are you sure you have the legitimate ST-Link? The ST drivers may detect the hacked serial number and refuse to work with illegal clones.
2022-06-26 09:32 PM
Thanks for your reply.
I started with an installed STM32CubeIDE/Programmer that did not work, later I did indeed install the .zip file you mentioned. My ST-LINK/V2 used to work before I upgraded to Windows 11. No idea, though, whether it is a legitimate device.