2022-04-09 02:50 AM
This is scheme for debug with swd
How to do active sw-dp with st-link v2 and stm32cubeProgrammer?
2022-04-09 03:01 AM
> when power is connected, the microcontroller is immediately in boot mode
How do you know it's in boot mode?
> St-link v2 also does not connect.
Try to connect under reset.
If you can connect through some of the bootloader protocols, check the option bytes.
JW
2022-04-09 03:25 AM
I add second question. Gow to do active sw-dp with st-link v2 and stm32cubeProgrammer?
2022-04-09 03:28 AM
Check a SWCLK pin it should be Pull-down at Reset state about 10K value.
2022-04-09 03:36 AM
Check part orientation
Check VDDA/VSSA
Check BOOT0
Check NRST
Check VTarget goes to pin 1 or 2 of ST-LINK
No magic options, should work out of the box unless something wrong with device.
2022-04-09 06:08 AM
i don't connect only vdda and vssa, is it problem? do you know, how to solve this problem? Not connecting in my PCB, i need to rebuild PCB?
2022-04-09 06:45 AM
VDDA/VSSA power the PLLs and POR circuits, not just DAC/ADC
Without power, will clamp device in reset, you'll see NRST held low
Perhaps you can solder on some fine wires to test/check
2022-04-13 07:16 AM
Hi @DPavl.1 ,
You can refer to AN4555 Getting started with STM32L4 Series and STM32L4+ Series hardware development for details about good setup mainly for power supply and debug management.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.