cancel
Showing results for 
Search instead for 
Did you mean: 

Nuceleo-F767ZI Board Meterial Test Report or Certification (UL)

JYun.5
Associate

hello.

I'm Jin, a medical device developer.

I am using Nucelo-F767ZI for the products under development.

If you need a flame retardant grade report for the board, please contact us.

I checked the site, but I can't find the PCB material report and flame retardant rating report, so I'm asking this.

Please reply after confirmation.

thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @JYun.5​, to the community!

NUCLEO boards are exclusively intended to be used for evaluating the respective STM32, for writing own software and thus for development until the own hardware has been developed. A flame retardant grade report should only be necessary for the own device, but according to the Evaluation Board Terms Of Use (also to be found on the NUCLEO-F767ZI website) no NUCLEO may be used in this own device..

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.