cancel
Showing results for 
Search instead for 
Did you mean: 

HSE on-board oscillator from X3 crystal (STM32 NUCLEO-H743ZI2)

HMsDobby2
Associate III

Hi

I use STM32 NUCLEO-H743ZI2 development board for my project. 
I'm considering purchasing electronic components for the first time, and I would appreciate a recommendation for an X3 crystal that could be used in this situation.

HMsDobby2_0-1712888661211.png

Additionally,

  • I understand that I should leave SB44 and SB46 as they are,
  • Solder and connect SB3 and SB4 each,
  • Solder 5.6pF capacitors to C69 and C70 each, and
  • Remove the 0-ohm resistor at SB45, correct?

My board is currently in this state,

HMsDobby2_4-1712889394585.pngHMsDobby2_5-1712889399353.png
and I plan to solder as described in the following diagram.

HMsDobby2_6-1712889650770.pngHMsDobby2_7-1712889660183.png

 

Thank you very much for your guidance.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @HMsDobby2 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

For a recomendations about the X3، i suggest you to take a look at the bill of material file of your board. You will find the recommended part. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @HMsDobby2 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

For a recomendations about the X3، i suggest you to take a look at the bill of material file of your board. You will find the recommended part. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you! However, can I just solder using the method I described? I'm a beginner and want to make sure.

Hello,


@HMsDobby2 wrote:

Thank you! However, can I just solder using the method I described? I'm a beginner and want to make sure.


Yes I confirm.

  • Leave SB44 and SB46 as they are,
  • Solder and connect SB3 and SB4 each,
  • Solder 5.6pF capacitors to C69 and C70 each, and
  • Remove the 0-ohm resistor at SB45

This is based on the schematics:

SofLit_0-1713359758377.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

Thanks for the detailed responses!