cancel
Showing results for 
Search instead for 
Did you mean: 

HSE on-board oscillator from X3 crystal (STM32 NUCLEO-H743ZI2)

HMsDobby2
Associate II

Hi

I use STM32 NUCLEO-H743ZI2 development board for my project. 
I'm considering purchasing electronic components for the first time, and I would appreciate a recommendation for an X3 crystal that could be used in this situation.

HMsDobby2_0-1712888661211.png

Additionally,

  • I understand that I should leave SB44 and SB46 as they are,
  • Solder and connect SB3 and SB4 each,
  • Solder 5.6pF capacitors to C69 and C70 each, and
  • Remove the 0-ohm resistor at SB45, correct?

My board is currently in this state,

HMsDobby2_4-1712889394585.pngHMsDobby2_5-1712889399353.png
and I plan to solder as described in the following diagram.

HMsDobby2_6-1712889650770.pngHMsDobby2_7-1712889660183.png

 

Thank you very much for your guidance.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @HMsDobby2 and welcome to the ST Community 😊.

For a recomendations about the X3، i suggest you to take a look at the bill of material file of your board. You will find the recommended part. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @HMsDobby2 and welcome to the ST Community 😊.

For a recomendations about the X3، i suggest you to take a look at the bill of material file of your board. You will find the recommended part. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you! However, can I just solder using the method I described? I'm a beginner and want to make sure.

Hello,


@HMsDobby2 wrote:

Thank you! However, can I just solder using the method I described? I'm a beginner and want to make sure.


Yes I confirm.

  • Leave SB44 and SB46 as they are,
  • Solder and connect SB3 and SB4 each,
  • Solder 5.6pF capacitors to C69 and C70 each, and
  • Remove the 0-ohm resistor at SB45

This is based on the schematics:

SofLit_0-1713359758377.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks for the detailed responses!