2020-11-04 02:38 AM
Hello Team,
I have to erase and program bin/hex file using ST-LINK Utility. I have ST-LINK V2 Programmer
I tried to install ST-LINK Utility on my computer, my package installer get stuck at last when I clicked on finish.
Package installation remains as it is on start bar until reboot.
After reboot I connect the target using ST-LINK V2 Programmer its get connected and able to read hex file.
I tried to erase the controller but getting following error
Then I checked in about info I get following info
I am able to connect with target but not able to perform any action. Please rectify the issue & suggest best way to program controller using GUI.
Installation package: en.stsw-link009.zip
OS: Windows10
Thanks,
2020-11-04 05:30 AM
> but getting following error
I don't see an error in your post.
You could also try STM32CubeProgrammer which does the same job but is better supported.
2020-11-04 09:35 AM
Hello @AJagt.2 ,
Welcome to the STM32 Community =)
I recommend you to follow this UM0892 User manual STM32 ST-LINK utility software description, in the "Getting started" section which describes the requirements and the procedures to install the STM32 ST-LINK utility software.
If your problem is not resolved, I advice you to download and use the STM32CubeProgrammer software tool for STM32 programming.
Hope this helps you.
When your problem is resolved, please close this thread by marking the Best answer.
Imen
2020-11-04 09:45 AM
>> I tried to erase the controller but getting following error
>> Then I checked in about info I get following info
It seems that your images are not inserted in the post.
You should click on [Image] icon (as you see below), then upload the image.
Imen
2020-11-04 09:57 AM
Make sure you have Admin rights.
Make sure there aren't any policy settings precluding the use of USB MSC devices.
Check that AV Software isn't interfering with application/driver installation.
2020-11-04 06:33 PM
This is the about info ST-LINK utility
Below is the error message when I tying to erase the program