2024-06-18 7:44 AM
I have the STEVAL-STWINBX1 development board and want to import the FP-SNS-DATALOG2 software into S32DS IDE so I can build and flash.
Is this possible and if so how ?
The user manual only mentions flashing the binary file STM32CubeProgrammer, but I would like to be able to modify the software and then flash it to the board using S32DS IDE
2024-06-18 8:09 AM - edited 2024-06-18 8:13 AM
User Manual UM3106, Getting started with the STM32Cube function pack for high speed datalogging and ultrasound processing
via:
https://www.st.com/en/embedded-software/fp-sns-datalog2.html#documentation
2024-06-18 8:29 AM
I was using the wrong IDE !
I was using "S32 Design Studio" instead of STM32 Cube IDE"
2024-06-18 8:38 AM
I am using a Segger J-Link Base to try and flash/debug the DATALOG2-STWIN.box application, but get the following warning...
If I select yes (multiple times) I then get the following error...
2024-06-18 8:42 AM
Seem to have fixed it, there was no power to the board (even though the battery was connected) so I powered the board via the USB connector