cancel
Showing results for 
Search instead for 
Did you mean: 

How to import software FP-SNS-DATALOG2 software to S32DS IDE so I can build and flash ?

johngj
Senior

I have the STEVAL-STWINBX1 development board and want to import the FP-SNS-DATALOG2 software into S32DS IDE so I can build and flash.

Is this possible and if so how ?

The user manual only mentions flashing the binary file STM32CubeProgrammer, but I would like to be able to modify the software and then flash it to the board using S32DS IDE

 

4 REPLIES 4
johngj
Senior

I was using the wrong IDE !

I was using "S32 Design Studio" instead of STM32 Cube IDE"

I am using a Segger J-Link Base to try and flash/debug the DATALOG2-STWIN.box application, but get the following warning...

johngj_1-1718724959595.png

johngj_0-1718724856009.png

 

If I select yes (multiple times) I then get the following error...

johngj_3-1718725040747.png

johngj_2-1718725021179.png

 

 

Seem to have fixed it, there was no power to the board (even though the battery was connected) so I powered the board via the USB connector