cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect STM32F103C8T6 to STLINK-V3MINIE

hafiqat_
Associate II

I recently bought a Blue Pill, STLINK-V3MINIE and an adapter. How do I connect them together correctly? 

photo_2025-03-23_12-42-46.jpg

5 REPLIES 5
STOne-32
ST Employee

Dear @hafiqat_ ,

 

You need just to connect/hook the SWD connector signals from the ST-link to the target : VDD, Ground , SWD and CLK 

IMG_2132.jpeg

Hope it helps you , pay attention on the orientation of the cable to not Have short circuit on both VDD/Ground .

STOne-32 

hafiqat_
Associate II

Do I just need to solder the contacts to the stlink? Without using an adapter?

Yes you can for development purposes . 

hafiqat_
Associate II

Where to solder SWDIO?

  ST-Link
+-----------+
|           |
|   Vtarget +<-------------------------+-----VDD
|           |                          |
|           |                          |
|           |                    +-----+-----+
|           |                    |           |
|     SWDIO +<------------------>+SWDIO      |
|           |                    |           | STM32 Target
|     SWCLK +------------------->+SWCLK      |
|           |                    |           |
| NRST +------------------->+NRST |
| | | | | | +-----+-----+ | | | | | | | GND +--------------------------+-----GND | | +-----------+