2017-10-02 11:58 PM
I'm trying to connect new ISOL version debugger to a device I have been debugging with the old ST-LINK. I do not have 20-pin JTAG on my device (small battery operated STM32L100) and I try to get only 3V3, GND, SWDIO and SWCLK connected. My problem is that the ten pin cable provided with the debugger fits to ST-LINK only one way and the User manual UM1075has a table 4.2 Connection with STM32 applications which suggests the pins would be 1, 20, 7 and 9 in the same order. Then again Figure 10. JTAG debugging flat ribbon layout shows that I should but the connector on the row where it doesn't fit because of the polarity pin. Which information do I trust now (and why would the 10 pin connector be fitted on the row that has only VCC and GND on it?) Anyone have a picture of the actual ST-LINK with the 4 wires connected?
#st-link-isol-pinoutSolved! Go to Solution.
2017-10-03 11:55 AM
Got this working now. Needed to connect 1, 3, 7, 9, 13 and 20 pins from JTAG to get this working.
2017-10-03 05:38 AM
OK, I figured out the pinout hopefully. The Jtag pinout seems to be correct Ijust took the 10 pin wire into pieces.
Now I still get stuck with output like this:
'STLINK GDB Server (EmBitz Dec 8 2016 12:12:38)
Shutdown after disconnect is active.Connected to STlink/V2 probe at 001:036
Chip ID is 00000429, Core ID is 2ba01477.Target voltage: 2.15Debugging enabled for all CPU modes.Number of HW-breakpoints: 0Listening at *:4242...GDB connected.'Well the voltage is 3,2V volts when measured from the board only, so the debugger is still
not correctly connected. It seems to be loading the device, the led on debugger is just blinking all the time.
Any ideas?
2017-10-03 11:55 AM
Got this working now. Needed to connect 1, 3, 7, 9, 13 and 20 pins from JTAG to get this working.
2018-01-15 08:54 AM
I have just got a v2-Isol and have similar problems.
I have target cables wired to the 20 way connector, using pins 1, 7,8,9,15. Worked find for years with an standard stlink v2. Swapping to the -Isol and it fails to connect to target.
I noticed you use 3 for reset (I use 15) and 13 for SWO which I do not use. Did you find that specific combination necessary?
I really don't want to modify all my target cables just to use a -Isol unit.........
2018-01-15 10:08 AM
A update, I have just used jumpers to test this out. Connected via swd stlink I find that I can use:
1: Vcc
7: SWDIO
9: SWCLK
15: NRST
For the standard STLink I can use any of the grounds but on the -ISol it will only connect if I use 10,12,14,18 or 20.
Tested on a F303RE (on a custom board) if it matters. Also tested on two STlink/V2-ISol adapters.
Maybe have missed something but I read the user guide 3 times and still can't find any reference to this fundamental difference between the two units. So that is two hours of my time I will not get paid for
:(
2018-09-28 05:29 AM
Plaese find below working cables connections for STlink/V2 ISOL:
I confirm that pin 4 is not working for GND.
You need to supply the target separately.
2019-07-26 01:17 AM
Thank you!
I use /V2 ISOL and I tried first to connect GND with pin 16, which is outpinned, so it cannot work! I didn't realize that I connected GND to the outpinned. This is also not mentioned in the documentation: "3. At least one of this pin must be connected to the ground for correct behavior (connecting all of them is recommended)." (UM1075)
ST, can you update the ST-LINK user manual with the particularities of the ST-LINK/V2 ISOL?
Best regards
Christoph