2025-03-24 11:11 AM
Hello. I was recently advised that STM32F103C8T6 and STLINK-V3MINIE should be soldered directly without an adapter.
VCC with 3V3
GND with GND
SWDCLK with CLK
SWDIO with ?
Solved! Go to Solution.
2025-03-24 11:38 AM - edited 2025-03-24 11:38 AM
> I was recently advised that STM32F103C8T6 and STLINK-V3MINIE should be soldered directly without an adapter.
This is not true. Using CN4 and a cable to a header on the board is the most common and often the best method.
> SWDIO with ?
SWDIO should be connected to pin 3, "TMS".
2025-03-24 11:38 AM - edited 2025-03-24 11:38 AM
> I was recently advised that STM32F103C8T6 and STLINK-V3MINIE should be soldered directly without an adapter.
This is not true. Using CN4 and a cable to a header on the board is the most common and often the best method.
> SWDIO with ?
SWDIO should be connected to pin 3, "TMS".
2025-03-24 1:41 PM - edited 2025-03-24 1:42 PM
@hafiqat_ However, you should be aware that you should buy the STM32F103C8T6 from authorised sources, otherwise the risk of getting counterfeits is almost 100%.
Problem: STMicroelectronics and its software cannot support them, which is why problems regularly occur when debugging and working (very often found here in the community). In such a case, you would have to contact the dealer or the manufacturer of the counterfeit.
2025-03-25 12:39 PM
> Using CN4 and a cable to a header on the board is the most common and often the best method.
I don't understand what CN4 is. Is it some kind of adapter? If so, what does it look like?