2022-01-26 03:22 AM
/home/i/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammer: line 4: 3947 Aborted (core dumped) $DIR/jre/bin/java -Djdk.gtk.version=2 -jar $DIR/STM32CubeProgrammerLauncher
this is the output I get to the terminal after the crash of the STM32CubeProgrammer. I have tested various versions of libusb, as well as Ubuntu 18 and Ubuntu 20. The result is always the same.What should I do to make STM32CubeProgrammer work on Linux? Is it possible?
2022-01-26 03:24 AM
tell me how to flash stm32H7 in the Linux console using st-link_v3?
2022-01-26 03:31 AM
STM32CubeProgrammer collapses from any action in its menu.
2022-01-26 03:33 AM
Ubuntu 18 and 20
2022-01-31 01:46 PM
the board was determined in STM32CubeProgrammer under Linux
2022-02-01 07:03 AM
CubeProgrammer appears to be increasingly sensitive to problems communicating with the target processor. It just crashes with no explanation. Do you have a Nucleo you can try first?
2022-02-01 11:04 AM
STM32CubeProgrammer saw the developer's board. now STM32CubeProgrammer does not break. If there are any successes in the work, I will let you know
2022-02-01 12:59 PM
ok