2023-03-06 04:18 AM
Hello circuit designers and PCB guys,
I have a problem of how to connect the H7 ethernet via a PHY and a ethernet USB bridge.
So I tested Microchip's LAN9512 ethernet-USB bridge on their dev board, that works great, see attached picture.
Problem:
I have to place the LAN9512 on the same PCB, and I must get rid of that extra RJ45/magnetics + cable (the red parts in the attached pic).
I must use as few components as possible, but how should I wire these parts without making it too dirty (it must work reliably and has to pass a EMI test someday...).
Any thoughts on that or other ideas?
Or experience with multiport PHYs like the LAN9303?
2023-04-11 09:59 AM
Hmmm, maybe I mis-understood your requirement. Do you need to keep the LAN8742->Magnetics->RJ45 path, and ADD the ability to connect LAN8742->LAN9512?
If so, can BOTH interfaces be active at the same time? That is not allowed without putting a hub/switch on the board (i.e. LAN9303 as you suggest).
2023-04-12 12:45 AM
The 2 interfaces would not be active at the same time.
Imagine a PoE supplied ethernet device (main use case, USB inactive), which can also be used with an ethernet-less laptop via USB.
So as soon as someone plugs in USB, the main ethernet path will be deactivated.
So, the only "clean" solution would be a dual PHY like LAN9303, no matter how I turn things around.
But your advice concerning the capacitive coupling, then between one port of the LAN9303 and the LAN9512, would be used.