cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO Pin not going High

jasd33p
Associate II

I'm using a Nucleo-H723VG board and trying to use the PB8 and PB9 pins. I'm able to set PB9 high and see a voltage of 3V but for PB8 it only shows a voltage of 359mv. I have tried enabling the internal pullup and still doesn't go high to 3V.

The yellow is PB9, which is going high and blue is PB8, only reads in mv range.

jasd33p_0-1725464875313.png

 

9 REPLIES 9
MM..1
Chief III

Are you sure your scope isnt 1:10

Yes there 1:1

Show photo board, i mean ST dont have VG nucleo, but ZG

And 1:1 on display is irelevant, check cable switch


@jasd33p wrote:

I'm using a Nucleo-H723VG board


Have you checked the board User Manual and/or Schematic to see if there's anything else using that pin?

 

PS

It looks like your scope has a USB socket:

AndrewNeil_0-1725466269773.png

You should be able to use that to download a proper screenshot - which will be much better than a wonky photo with reflections, etc!

Imen.D
ST Employee

Hello @jasd33p  

Ensure that there are no conflicts with other peripherals or pin configurations that might be affecting the GPIO pin (check if the pin is also used for another alternate function)

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
SofLit
ST Employee

Hello,

On which connector and which pin you are probing PB8? CN9/11? or CN12/3?

On CN9/11, the solder bridge is not soldered.

SofLit_0-1725466504633.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Sorry meant ZG

I was probing PB9 on CN7

jasd33p_0-1725466676838.png

 

SofLit
ST Employee

@jasd33p wrote:

I have tried enabling the internal pullup and still doesn't go high to 3V.

 

Hope you didn't broke the IO!

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.