2024-09-24 01:55 PM
I have been sitting on this problem for a couple of days where I have been trying to use f_mount on a 8GB SD card (I formatted it to FAT32 and to a sector size of 4096.) I am also copying a very popular library by eziya: https://blog.naver.com/eziya76/221188701172. The chip I am using on my NUCLEO board is a STM32F103RB.
Although the program is very simple, no matter what I do, the SD card never gets mounted. When trying to read the available space and the total space, it always returns 0.
Here is my code for the main loop:
FATFS fs; FIL fil; FRESULT fresult; char buffer[1024]; UINT br, bw; FATFS *pfs; DWORD fre_clust; uint32_t total, free_space;
fresult = f_mount(&fs, "", 1); printf("%d \n", fresult); if (fresult != FR_OK) printf("Unsuccessful again\n"); else printf("Mounted successfully! \n"); f_getfree("", &fre_clust, &pfs); total = (uint32_t)((pfs->n_fatent - 2) * pfs->csize * 0.5); printf("Total size: \t%lu\n",total); free_space = (uint32_t)(fre_clust * pfs->csize * 0.5); printf("SD CARD free space: \t%lu\n", free_space);
I used SPI for the configuration, here are my configurations for the CubeIDE:
SPI configuration:
FATFS configuration:
The SPI pinout in CubeIDE:
I set the CS output on default high for the SPI communication protocol.
The clock configuration:
I use this SD card reader module
What I have tried and didn't work:
Switch out the SD card reader module.
Switch out the microSD card.
Use an internal Pull-up resistor for the MOSI and CS lines (I didn't have an option to choose pull-up resistors. for MISO and SCK.)
Have "Low" as default CS output.
Checked the SCK signal on the oscilloscope and it was reading something, which seemed to me alright, so I don't think it's a hardware issue.
Put some signs into the "" of the f_mount input.
Use 0 as the initialization input for the f_mount function (this returns always FR_OK though, so it doesn't really help.)
Double check SPI connections (everything should be connected correctly.)
Any help is welcome, thank you so much!
Solved! Go to Solution.
2024-09-25 10:00 AM - edited 2024-09-25 10:01 AM
Hello @Nxyoutou and welcome to the community,
I propose you to look at the Adafuit SD implementation (using SPI) provided in STM32CubeF1 BSP: in https://github.com/STMicroelectronics/STM32CubeF1/blob/master/Drivers/BSP/Adafruit_Shield/stm32_adafruit_sd.c
2024-09-25 10:00 AM - edited 2024-09-25 10:01 AM
Hello @Nxyoutou and welcome to the community,
I propose you to look at the Adafuit SD implementation (using SPI) provided in STM32CubeF1 BSP: in https://github.com/STMicroelectronics/STM32CubeF1/blob/master/Drivers/BSP/Adafruit_Shield/stm32_adafruit_sd.c