cancel
Showing results for 
Search instead for 
Did you mean: 

External STLink V2 connection to Nucleo-STM32H723ZG

Davit_Imnaishvili
Associate II

Hello, the embedded STLink of my  Nucleo-STM32H723ZG board has stopped functioning when I was trying to set up the Vref and I'm trying to use an external STLink V2 programmer to write code into the microcontroller. The problem is that I can't find the proper connection instructions in any of the manuals. Here are the 10 pins of my regular STLink V2 programmer:

RST, SWDIO
GND, GND

SWIM, SWCLK

3.3V, 3.3V
5V, 5V

 

Where do I have to connect the pins of STLink on this board?

 

Screenshot 2024-08-15 at 6.37.34 PM.png

2 REPLIES 2
LCE
Principal

UM2407, page 17 - use the MIPI-10 debug connector, but first check the jumper.

I have that board, but I haven't tried that!

LCE_0-1723734750136.png

 

Peter BENSCH
ST Employee

@Davit_Imnaishvili But please make sure that you don't try one of those colourful tin can ST-LINK/V2, because they are fakes with fake MCUs and usually don't work. There are plenty of discussions about this here in the community, as well as a knowledgebase article.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.