cancel
Showing results for 
Search instead for 
Did you mean: 

Extend FP-SNS-DATALOG2 / Phython SDK to support an additional external sensor.

Ferag
Associate

Hi ST Team

I have added a sensor implementation to the FP-SNS-DATALOG2 (2 D movement tracking sensor PAT9136) in order to be able to record position data together with MEMS sensor data. This works well for data recording/retriving to/from the SD card. Now I would like to extend the Python GUI application (hsdatalog_GUI.py) with an additional plot to be able to display live data when connected by USB. I took a look on the implementation an I cannot figure out how to deal with related FP_SNS_DATALOG2_Datalog2-4.json file, which seems to be automaticaly generated. Can you expose me how to proceed?

Thanks in advance!

Ludwig

1 REPLY 1
SimonePradolini
ST Employee

Hello @Ferag 

I saw your issue on github: https://github.com/STMicroelectronics/fp-sns-datalog2/issues/10

Can we merge the two requests and continue the discussion only on github?

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.