2021-04-14 04:21 AM
When I tried to debug my STM32F303RE nucleo board with Truestudio , I get this messages from console:
When I get this message , I was working on EXTI interrupts at register level
STMicroelectronics ST-LINK GDB server. Version 5.1.0
Copyright (c) 2018, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : D:\projeler\sf_projeler\Attolic_workspace\EXTI2_example\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Hardware watchpoint supported by the target
SWD frequency = 4000 kHz
ST-LINK Firmware version : V2J37S27
Device ID: 0x446
PC: 0xfffffffe
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Failed to bind to port 61234, error code -1: No error
Failure starting GDB server: TCP port 61234 not available.
I was able to program it even last night , but this morning suddenly occur this error.
Now , I can program it with stm32cube programmer .
What I did to solve it:
thanks.
Solved! Go to Solution.
2021-04-14 05:52 AM
SOLVED!!
It is solved again suddenly :D :D :D
I writed this post and ı walked at park about 1-2 hours.
When I checked again , I surprised .
Anyone can explain why happend this ?
-met
2021-04-14 05:52 AM
SOLVED!!
It is solved again suddenly :D :D :D
I writed this post and ı walked at park about 1-2 hours.
When I checked again , I surprised .
Anyone can explain why happend this ?
-met