2021-04-13 3:39 AM
I performed the following steps:
1) Set JP7 to STLK
2) Connect USB -> Demo starts correctly
3) Flash a simple self-written code (sets LED to state of user-button) via OpenOCD -> ST-Link works
4) Flash a second self-written code (sets both LED to state of user-button) via OpenOCD -> works -> my own code did not break flashing
5) Performed Steps 1-4 with a second Eval board -> works
6) Copied the OpenOCD config twice and added the two serial numbers of the boards
7) Connected both boards via USB (no other connection) and tried adressing them separately -> did not work
8) Disconnected both boards, reconnected one, retried step 4 -> did not work. The button/LED-Program does not work any more.
Since I couldn't rule out damages like ESD, I bought two new boards.
9) Flashed board #3 -> works
10) Flashed board #4 -> works
11) Connected boards #3 and #4 (connected with CAN-wires in this case) WITHOUT flashing -> boards don't start up any more
12) STM32CubeProgrammer does find the ST-LINK, but not the MCU.
Further notes:
* Pressing the reset button does not change anything on the boards now.
* Holding reset during CubeProgrammer run has no effect.
* Specifying -rst or -hardRst has no effect.
* The flashing itself does not seem to be the problem, because it occurred between two steps where no flashing occurred.
* Since it is reproducible by connecting two boards, external influences can be dismissed.
* Output of CubeProgrammer and dmesg:
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0
-------------------------------------------------------------------
ST-LINK SN : 004500413438510C34313939
ST-LINK FW : V3J7M2
Board : STM32H735G-DK
Voltage : 3,29V
Error: No STM32 target found!
2nd connect tentative with a lower frequency (8MHz)
ST-LINK SN : 004500413438510C34313939
ST-LINK FW : V3J7M2
Board : STM32H735G-DK
Voltage : 3,30V
Error: No STM32 target found![624399.372547] usb 1-2: new high-speed USB device number 90 using xhci_hcd
[624399.521018] usb 1-2: config 1 interface 2 altsetting 0 endpoint 0x84 has an invalid bInterval 255, changing to 11
[624399.521497] usb 1-2: New USB device found, idVendor=0483, idProduct=374e, bcdDevice= 1.00
[624399.521501] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[624399.521504] usb 1-2: Product: STLINK-V3
[624399.521506] usb 1-2: Manufacturer: STMicroelectronics
[624399.521508] usb 1-2: SerialNumber: 003200273438510734313939
[624399.539360] usb-storage 1-2:1.1: USB Mass Storage device detected
[624399.539572] usb-storage 1-2:1.1: device ignored
[624399.553135] cdc_acm 1-2:1.2: ttyACM0: USB ACM device
[624405.442207] usb 1-2: USB disconnect, device number 90
[624413.572612] usb 1-2: new high-speed USB device number 91 using xhci_hcd
[624413.721031] usb 1-2: config 1 interface 2 altsetting 0 endpoint 0x84 has an invalid bInterval 255, changing to 11
[624413.721513] usb 1-2: New USB device found, idVendor=0483, idProduct=374e, bcdDevice= 1.00
[624413.721517] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[624413.721520] usb 1-2: Product: STLINK-V3
[624413.721522] usb 1-2: Manufacturer: STMicroelectronics
[624413.721525] usb 1-2: SerialNumber: 003200273438510734313939
[624413.739405] usb-storage 1-2:1.1: USB Mass Storage device detected
[624413.739733] usb-storage 1-2:1.1: device ignored
[624413.753289] cdc_acm 1-2:1.2: ttyACM0: USB ACM device
[624526.776538] usb 1-2: USB disconnect, device number 91
[624558.720923] usb 1-2: new high-speed USB device number 92 using xhci_hcd
[624558.873348] usb 1-2: config 1 interface 2 altsetting 0 endpoint 0x84 has an invalid bInterval 255, changing to 11
[624558.873833] usb 1-2: New USB device found, idVendor=0483, idProduct=374e, bcdDevice= 1.00
[624558.873837] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[624558.873840] usb 1-2: Product: STLINK-V3
[624558.873843] usb 1-2: Manufacturer: STMicroelectronics
[624558.873846] usb 1-2: SerialNumber: 003200273438510734313939
[624558.892870] usb-storage 1-2:1.1: USB Mass Storage device detected
[624558.893205] usb-storage 1-2:1.1: device ignored
[624558.917493] cdc_acm 1-2:1.2: ttyACM0: USB ACM device
[624591.435057] usb 1-2: USB disconnect, device number 92
[624611.384936] usb 1-1: new high-speed USB device number 93 using xhci_hcd
[624611.533421] usb 1-1: config 1 interface 2 altsetting 0 endpoint 0x84 has an invalid bInterval 255, changing to 11
[624611.533904] usb 1-1: New USB device found, idVendor=0483, idProduct=374e, bcdDevice= 1.00
[624611.533907] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[624611.533911] usb 1-1: Product: STLINK-V3
[624611.533913] usb 1-1: Manufacturer: STMicroelectronics
[624611.533916] usb 1-1: SerialNumber: 003200273438510734313939
[624611.896936] usb-storage 1-1:1.1: USB Mass Storage device detected
[624611.897262] usb-storage 1-1:1.1: device ignored
[624611.929503] cdc_acm 1-1:1.2: ttyACM0: USB ACM device
[624625.020963] usb 1-2: new high-speed USB device number 94 using xhci_hcd
[624625.169325] usb 1-2: config 1 interface 2 altsetting 0 endpoint 0x84 has an invalid bInterval 255, changing to 11
[624625.169805] usb 1-2: New USB device found, idVendor=0483, idProduct=374e, bcdDevice= 1.00
[624625.169809] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[624625.169812] usb 1-2: Product: STLINK-V3
[624625.169814] usb 1-2: Manufacturer: STMicroelectronics
[624625.169817] usb 1-2: SerialNumber: 004500413438510C34313939
[624625.533826] usb-storage 1-2:1.1: USB Mass Storage device detected
[624625.534232] usb-storage 1-2:1.1: device ignored
[624625.534745] cdc_acm 1-2:1.2: ttyACM1: USB ACM device
[624631.559510] usb 1-2: USB disconnect, device number 94
[624636.444603] usb 1-1: USB disconnect, device number 93
[624649.009002] usb 1-1: new high-speed USB device number 95 using xhci_hcd
[624649.157507] usb 1-1: config 1 interface 2 altsetting 0 endpoint 0x84 has an invalid bInterval 255, changing to 11
[624649.158122] usb 1-1: New USB device found, idVendor=0483, idProduct=374e, bcdDevice= 1.00
[624649.158123] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[624649.158123] usb 1-1: Product: STLINK-V3
[624649.158124] usb 1-1: Manufacturer: STMicroelectronics
[624649.158124] usb 1-1: SerialNumber: 004500413438510C34313939
[624649.521403] usb-storage 1-1:1.1: USB Mass Storage device detected
[624649.521754] usb-storage 1-1:1.1: device ignored
[624649.522314] cdc_acm 1-1:1.2: ttyACM0: USB ACM device
Solved! Go to Solution.
2021-04-13 6:17 AM
Are these boards powered from the same power domain, with well bonded common grounds?
You could try Switching (SW1?) the boards to boot from ROM (BOOT0=HIGH), completely cycle the power (removed ALL connections) a couple of times, and then see if the STM32 Target can be found, if so erase the device.
2021-04-13 6:17 AM
Are these boards powered from the same power domain, with well bonded common grounds?
You could try Switching (SW1?) the boards to boot from ROM (BOOT0=HIGH), completely cycle the power (removed ALL connections) a couple of times, and then see if the STM32 Target can be found, if so erase the device.
2021-04-13 7:39 AM
The first time, the boards did not have any direct connection. Both only had the single USB connection to the PC.
I tried your suggestion and I was able to perform a full erase and now I can get a connection again. Thank you a lot!
Digging more, I found out that this deadlock seems to be common when messing up the SMPS/LDO configuration: https://community.st.com/s/question/0D50X0000BD2xd9/cubemx-is-missing-the-pwrdirectsmpssupply-option-under-rccsupplysource
Apparently, it wasn't because I connected two boards, but because I disconnected/power-cycled them during this process.
I took the default parameters from the discovery kit example provided by CubeMX - but apparently they don't work...
2021-04-14 5:48 AM
Hi @KNeus.1 ,
I suggest you have a look to this article, it contains some explanations.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.