cancel
Showing results for 
Search instead for 
Did you mean: 

Developing a circuit based on STM32 for a medical device application

MG_Tech
Associate

I have tested the POC (Proof of Concept) by using 'Nucleo-439ZI' evaluation Board. I am now going to use the same schematics as reference for my prototype and create a custom board by removing the Morpho and Zio connectors as well as the unintended functions. 

I will be using this board for a medical application wherein compliance with ' IEC60601 Standard' is mandatory. I would like to know if any additional circuity need to be added to the schematics attached apart from adding TVS diodes at the I/O pins for protection from surge voltages. 

Thanks

 

 

 

 

2 REPLIES 2
CTapp.1
Senior

I would start by looking at what IEC60601 says.


@MG_Tech wrote:

for a medical application wherein compliance with ' IEC60601 Standard' is mandatory.


You'll be needing to get compliance certified, then?

Compliance labs will usually provide consultancy prior to testing - for a fee.

This is way beyond the scope of a forum!