2021-04-08 11:22 PM
I destroyed the MCU(STM32H743ZIT6) and ST-Link V3.
But I don't know what happen.
When I connect the ST-LinkV3 with the Laptop, then the ST-Link and MCU was broken.
So, if you know what happen, please teach for me.
2021-04-08 11:45 PM
The same thing happened to me too.
With an STM32H735-DK. One day, I turn on it but it didn't run. The integrated ST-Link V3 seems to work correctly (I can connect it to the PC) but the STM32H735 does work: it not run and I cannot program it. The day before everything was working fine !!!! I didn't understand what could have happened.
2021-04-09 1:03 AM
Thank you for reply!
I resolve this problem.
This problem is made by some causes, I found these causes.
2021-04-09 6:55 AM
It is very very rare that breackage happens out of the blue. In most cases something happened, e.g.:
So carefully think about what you did since you last handled the board. Is the Stlink still recognized? Is the board still powered(green led) ? ...
Otherwise, when y
2021-04-09 6:55 AM
It might be helpful for others in the future if you share what caused your issue.
2021-04-09 7:08 AM
Takes some skillz
At the places I've worked there's usually a guy with the Technology Kiss of Death, who can break pretty much any hardware or software if left alone with it even briefly..
2021-04-09 7:11 AM
The H7 can be bricked by incorrect LDO/SMPS and VOS settings.
The NRST is not a true reset in the classic sense.
One of the tricks to un-brick the H7 is to pull BOOT0 HIGH, and then cycle the power completely a couple of times, ie fully disconnect and reconnect the USB/Power from the device. Then connected and erase with BOOT0 still HIGH, stopping broken code on the device from running
2021-04-09 7:13 AM
I think so too.
This is embarrassing, but I can't speak English well.
So, I can't speak well about the detail.
Its cause, short circuit between the ST-Link and MCU through the electrical outlet.
So, it isn't concern about ST.
I'm so sorry.
And thank you for any reply.
2021-04-09 7:31 AM
Hi.
For me, the USB cable is ok because with other board it works correctly.
The power source is the USB
The LD5 and LD6 are ON
With ST-Link Upgrade Utilities I can connected to ST-LINK V3 (inside on the board STM32H735-DK) and upgrade it to last version (V3.J7.M2); but when with STM32CubeProgrammer the message "Error: NO STM32 target found!" will be displayed.
The display backlight is on (also when I press the RST button).
If I try press "Run Target" from TouchGFX, I read the following messages:
ST-LINK SN : 001C003F3438510534313939
ST-LINK FW : V3J7M2
Board : STM32H735G-DK
Voltage : 3.29V
Error: No STM32 target found!
c:/works/ST/ConfIndustries_0/gcc/include/flash_sections_int_ext.mk:2: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 1
../gcc/Makefile:52: recipe for target 'flash' failed
With STM32CubeIDE I read the messages:
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
Thanks.
2021-04-09 7:42 AM
Please check that JP7 is in position 1-2.
+ Try to connect under reset.