cancel
Showing results for 
Search instead for 
Did you mean: 

Controlling STM32F407 bootloader (Discovery board) with another board

ATank.1
Associate III

Hello 

I think we can control the reset and boot0 pin of F407 externally through a different board STM32H745 disco. I want to put the F407 in boot mode and send data to program the F405 through UART. Please confirm

Thanks & Regards,

Anuj

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @ATank.1 ,

According to that board schematics, you can drive the BOOT with a GPIO from STM32H745 as BOOT pin is exported on the P2 connector:

SofLit_0-1729516805512.png

But you need to unsolder SB18 and R31.

For the reset, same thing, it's exported on the P1 connector, but you need to unsolder SB1:

SofLit_1-1729517041429.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

2 REPLIES 2
SofLit
ST Employee

Hello @ATank.1 ,

According to that board schematics, you can drive the BOOT with a GPIO from STM32H745 as BOOT pin is exported on the P2 connector:

SofLit_0-1729516805512.png

But you need to unsolder SB18 and R31.

For the reset, same thing, it's exported on the P1 connector, but you need to unsolder SB1:

SofLit_1-1729517041429.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hi @SofLit 

Thank you for the quick response. This is exactly what I was looking for.

Regards,

Anuj