2024-09-02 9:49 AM - last edited on 2024-09-06 9:42 AM by mƎALLEm
Im using NUCLEO-H755ZI-Q. I used it together with plattformio and arduino framework. In order to get arduino to work im using this setup:
[env:nucleo_h743zi]
platform = ststm32
board = nucleo_h743zi
framework = arduino
monitor_speed = 115200
Error: init mode failed (unable to connect to the target)
As well as the board is not connected stm32CubeProgrammer.
Solved! Go to Solution.
2024-09-06 1:15 PM - edited 2024-09-06 1:17 PM
Yes NUCLEO-H745ZI-Q but dioesnt support arduino framework. What aboutwhat about something like Nucleo-F767ZI or NUCLEO-H753ZI? Are these both fully supporting arduino framework? Then maybe that would be an alternative. My criteria is the fastest board possible with about 100 gpio