2020-08-17 7:03 AM
On Windows 10, I just updated (again) to the 1.4.2 version, hoping to solve this issue, yet nothing changed.
Already tried a clean install (again) and re-installed the latest STM32CubeProgrammer: nothing changed.
Will ST handle this sooner or later please? Or at least give some help in diagnosing the problem? Thanks
Solved! Go to Solution.
2020-12-16 10:06 AM
I have had the same problem, and following the installation instructions of the dll file, everything works fine now.
Thanks.
2020-12-17 12:47 AM
Hi,
You can install (not update) STM32CubeIde v1.5.0, the new libusb dll is installed now.
Rgds,
Laurent
2020-12-20 10:48 AM
Good day! I faced a similar problem in STM32CubeIDE version 1.5.0, but with another ST-Link firmware version: "V2J37A1 - STM32 Debugger + Audio(VCP)". STM32CubeIDE is giving error message: "No ST-LINK detected! Please connect ST-LINK and restart the debug session".
I tried to solve this problem according the advices in this topic and updated stlink-server from the newest version, but it didn't work. After that I have changed files in folder "stlink_server" on older version, and my ST-Link has worked!
Can you solve this problem with firmware version "V2J37A1 - STM32 Debugger + Audio(VCP)" in the next version of STM32CubeIDE, please?
Thanks for your support!)
2022-01-22 8:26 AM
So is there any fix for this yet?
STM32CubeProgrammer 2.9.0 can't even detect the L031K6 nucleo st link.
STM32CubeIDE 1.8.0 does see it but won't use it.
Fortunately I can update it to mass storage mode, that works, but debugging would be nice.
2023-08-05 6:25 AM
Hi,
I have installed latest version of STM32CubeIDE which is 1.13.1. I am facing the same problem of ST-Link not detected. I tried solving the issue following your guides but it's not being resolved. If you could please guide me how can I resolve this issue. I would be really grateful.