Hello,I am pretty sure you have to look at the schematic of the nucleo, there is a solder bridge to set or to remove.I don't have the board here to look but I am sure I did a hardware modification for the swo pin to be redirected to the STLink.I just...
Hello,I think the Ram was restricted to 128K as the device has 128K of Flash.In order to not create a project in the whole RAM and then it wouldn't fit into flash.Anyway, the RAM linker scripts are given besides the Flash linker scripts, they are not...