cancel
Showing results for 
Search instead for 
Did you mean: 

break implementation - ADC on stm32c031c6 using CubeMX

dee1
Associate II

please provide me the information about how to implement break for adc input, give me one example for break implementation in stm32c031c6 with mxcube configuration 

9 REPLIES 9

@dee1 wrote:

 break for adc input 


What do you mean by that ?

how to give break input,or how to inactive/disable pwm output by using break function

 

dee1
Associate II

i used complementary pwm channels of tim1,break implementation for those channels,how to configure in mxcube and HAL for that.

Not sure how that applies to an ADC input ?

:thinking_face:

UM3029 is the Description of STM32C0 HAL and low-layer drivers:

https://www.st.com/resource/en/user_manual/um3029-description-of-stm32c0-hal-and-lowlayer-drivers-stmicroelectronics.pdf

via: https://www.st.com/en/embedded-software/stm32cubec0.html#documentation

 

dee1
Associate II

is this not understanding?

can you provide example for timer break input implementation

 

In the 'C0 family, there's no hardware to generate Break in TIM1 from ADC input.

JW

but for tim1 pwm generation channel break is there,i want for that how to use break

 

I don't use the 'C0 family and I don't use CubeMX/Cube, but basically, you set up TIM1_BKIN pin (e.g. PA6) to the appropriate AF, and in TIM1_BDTR enable Break by setting the BKE bit. Optionally you can also change the polarity and add filtering, set up the output pins behaviour etc. in other bits of TIM1_BDTR - see description of that register in RM, and read functional description in Using the break function in the TIM chapter in RM.

JW