2022-09-16 03:58 AM
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
2022-09-16 05:45 AM
Hallo @kabid.1 ,
I advise you to refer to this FAQ: How to solve debugger connection issues.
Check if all jumpers are correctly configured.
Try using latest release of STM32Cubeprogrammer, and make sure to upgrade the ST-LINK/V2-1 firmware.
Try connect to "Under reset" mode.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen