cancel
Showing results for 
Search instead for 
Did you mean: 

Advice for Adding cellular connectivity

Fates
Associate II

I have a dev_kit which I want to use to connect to a cellular network with LTE-M. But the example-file that they gave were a .bin file from XCUBE_CELLULAR for B-L462E-CELL1\cellular. Since I never used i, I have no clue what to do. How could I get started with the modem and get a connection with a network. So that I can send and receive data? OR something like the project-example they gave to us. That would also help. 

 

Thank you!

0 REPLIES 0