cancel
Showing results for 
Search instead for 
Did you mean: 

ADC voltage drop

xeng_EE
Associate

Hi I have been seeing voltage spikes and drops on the signals coming from the ADC. I'm not sure what is happening and wanted to see if anyone else has seen this before. Spikes.PNG

3 REPLIES 3
Karl Yamashita
Lead III

The ADC is an input so why would there be signals be coming from the ADC?

Now if that graph is the readings from the ADC and you're outputting the values to the PC?, then more than likely an issue with the HW that the ADC is picking up. 

Tips and Tricks with TimerCallback https://www.youtube.com/@eebykarl
If you find my solution useful, please click the Accept as Solution so others see the solution.

@xeng_EE wrote:

Hi I have been seeing voltage spikes and drops on the signals coming from the ADC.


So have you looked at the input signal to the ADC - does it have corresponding "spikes and drops" ?

Imen.D
ST Employee

Hello @xeng_EE and welcome to the Community, 

Make sure to respect the ADC characteristic values in the datasheet: having the adequate sampling time, the right input impedance, with stable VDDA and VREF+ voltages.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen