cancel
Showing results for 
Search instead for 
Did you mean: 

关于STM32G030芯片的�?��?上的在线烧录问题

Ayang.1
Associate II

你好,关于STM32G030在PCBA�?��?上的在线烧录,想知�?�是下载什么软件�?�烧录? 用的工具是ST-Link V2�?�以�?�?还有如果芯片程�?加密�?护了�?怎么解�?�?能用ST-Link V2�?�烧录?

或者�?�以推�??�?�外一款USB在线烧录工具能满足�?求, 谢谢。

11 REPLIES 11
Ayang.1
Associate II

Hi @Imen DAHMEN​  your STMCubeprogrammer msut first click "Connect" it will read the chip type and merory automactially if connected sucessfully. You can tyr it your programming software if can do "uncheck" function.

Houda GHABRI
ST Employee

Hi @Ayang.1​ ,

This error message is "normal" we cannot read Data when read out protection is equal to 1 (0xBB).

So you need just to click OK to the message then go to Option bytes Tab and modify the RDP value.

Can you please test and tell me if it is Ok?

Houda